4.12 ATWILC Baremetal v3.4
The following are bug fixes and enhancements for RTP:
- SDIO porting example for SAM4s
- BLE/BT Firmware download and start
- Implemented
m2m_coex_set_mode(tenuCoexMode enuCoexMode)to switch the tuner between:M2M_COEX_MODE_WIFI- tuner operates in Wi-Fi only modeM2M_COEX_MODE_BT- tuner operates in BT/BLE only modeM2M_COEX_MODE_COMBO- tuner arbitrates access to the tuner between Wi-Fi and BT/BLE
- Add error handling in the SPI if the command does not equal the response till the timeout
- Added SDIO interface support for SAM4S MCU
- Fix unaligned buffers issue for SDIO
- Download and start BLE firmware
- Implement Wi-Fi/BLE Coexistence