1.3.5.3.11 MAC_ESTABLISH_CONFIRM_CB Function Pointer
C
typedef void (*MAC_ESTABLISH_CONFIRM_CB)(uint16_t conHandle,
MAC_ESTABLISH_CONFIRM_RESULT result, uint8_t *eui48, uint8_t type,
uint8_t *data, uint16_t dataLen, uint8_t ae);
Summary
Callback function pointer for the MAC connection establishment confirm.
Description
This callback is used for the MAC connection establishment confirm.
- conHandle: Unique identifier of the connection
- result: Result of the connection establishment process
- eui48: Pointer to the address of the node to which this connection will be addressed
- type: Convergence Layer type of the connection
- data: Data associated with the connection establishment procedure
- dataLen: Length of the data in bytes
- ae: Flag to indicate that authentication and encryption is requested (v1.4)
Remarks
None.