1.3.5.6.62 BMNG_PPROF_GetZcDiffRequest Function

C

void BMNG_PPROF_GetZcDiffRequest(uint8_t cmd, uint8_t *eui48);

Summary

Requests to get the zero cross difference between BN and SN using the PRIME Profile.

Description

This routine requests to get the zero cross difference between BN and SN using the PRIME Profile.

Precondition

None.

Parameters

ParametersDescription
cmdCommand to acknowledge
eui48Pointer to the address of the node to be asked

Returns

None.

Example

uint8_t eui48[6];
memset(eui48, 0x12, 6);
    
BMNG_PPROF_GetZcDiffRequest(PPROF_GET_ZC_DIFF_REQUEST, eui48);

Remarks

The command is acknowledged with the PPROF ACK callback.

The result of the request is returned in the PPROF zero cross difference response indication callback.