1.3.5.6.61 BMNG_PPROF_GetEnhancedRequest Function
C
void BMNG_PPROF_GetEnhancedRequest(uint8_t cmd, uint8_t *eui48, uint16_t dataLen,
uint8_t *data);
Summary
Requests to get a PIB attribute from a node using the PRIME Profile.
Description
This routine requests to get a PIB attribute from a node using the PRIME Profile.
Precondition
None.
Parameters
| Parameters | Description |
|---|---|
| cmd | Command to acknowledge |
| eui48 | Pointer to the address of the node to be asked |
| dataLen | Data length |
| data | Pointer to the data |
Returns
None.
Example
uint8_t data[3] = {0x00, 0x20, 0}; uint8_t eui48[6]; memset(eui48, 0x12, 6); BMNG_PPROF_GetEnhancedRequest(PPROF_GET_ENHANCED_REQUEST, eui48, sizeof(data), &data);
Remarks
The command is acknowledged with the PPROF ACK callback.
The result of the request is returned in the PPROF enhanced response indication callback.