32.6.6 Low-Pass Filter Mode
The Low-Pass Filter mode (MD =
100) acts similarly to the Average mode in how it
handles samples (accumulates samples until the ADCNT value is greater than or equal to
ADRPT, then triggers threshold comparison), but instead of a simple average, it performs a
low-pass filter operation on all of the samples, reducing the effect of high-frequency
noise on the average, then performs a threshold comparison on the results. In this mode,
the CRS bits
determine the cut-off frequency of the low-pass filter.