5.1.2.7 ZDO_GetNeibTable Function
Syntax
void ZDO_GetNeibTable(ZDO_Neib_t *table);
Description
This function retrieves the neighbor table.
The function writes the contents of the neighbor table to the buffer specified by a pointer to it.
Note: Not all entries of the neighbor table are included, namely only neighbors with RELATIONSHIP_PARENT, RELATIONSHIP_CHILD and RELATIONSHIP_NONE_OF_ABOVE relationships are included (in addition, this implies that information about unauthenticated children is not retrieved).
The space for the buffer must be allocated at compile time; that is, the variable for the buffer must be declared as static. The following code example demonstrates a typical way to call the function:static ZDO_Neib_t neighborTable[CS_NEIB_TABLE_SIZE]; // Buffer for the neighbor table ... ZDO_GetNeibTable(neighborTable);
Input Parameters
| Parameter Name | Description |
|---|---|
table | Pointer to store the address of the neighbor table |
Return Type and Values
- None