6.9 Program SPI Flash Image
(Ask a Question)To program SPI Flash Image, perform the following steps:
- Double click Generate SPI Flash Image and right click Run PROGRAM_SPI_IMAGE Action to get the SPI Flash programmed with the application as shown in the following figure.Important: If you want to program the external SPI Flash using the
.jobfile instead, see Appendix: Programming the Device Using FlashPro Express, page 41.Figure 6-7. SPI Flash Programming 
- Power-cycle the board after you program the PolarFire device and the external SPI Flash.
The demo is ready to be run. For information about how to run the demo, see Running the Demo.