6.8 Run PROGRAM Action
(Ask a Question)After generating the bit stream, the PolarFire device must be programmed. Follow these steps to program the PolarFire device using the Libero design flow:
Note: If you want to program the PolarFire FPGA using the
.job file instead, see Appendix 3: Programming the Device and External SPI FlashPro Express.- Ensure that the jumper settings on the board are as listed in the following table.
Table 6-2. Jumper Settings Jumper Setting J18, J19, J20, J21, and J22 Close pins 2 and 3 for programming through FTDI J28 Close pins 1 and 2 for programming through the on-board FlashPro5 J4 Close pins 1 and 2 for switching the power manually using SW3 J12 Close pins 3 and 4 for 2.5V - Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the host PC to J5 Future Technology Devices International Limited (FTDI) port on the board.
- Connect any one of the open network 1G Ethernet capable ports to the J15 connector (RJ45-PORT 0) on the board.
- Power-up the board using the SW3 slide switch.
- On the Libero Design Flow tab, double click Run PROGRAM Action.
When the device is successfully programmed, the LEDs 6 and 7 on the board glow, and a green tick appears, as shown in the following figure.
Figure 6-6. Run Program Action 
- Right click Run Program Action and select View Report to view the corresponding log file in the Reports tab.