18.5.4 Integration of the Multiple Samples
In Integration of the Multiple Samples Example, the conversions are started by a software trigger and continued by back-to-back triggers until the number of conversions is less than set in the AD1CNT15 register.
Integration of the Multiple Samples Example
#include <xc.h>
// The channel output.
long result = 0;
int main() {
// In this example channel 15 will be used.
// Integration conversion mode.
AD1CH15CONbits.MODE = 2;
// Set number of conversions accumulated to 123.
AD1CH15CNT = 123;
// Software trigger will start a conversions.
AD1CH15CONbits.TRG1SRC = 1;
// Re-trigger back to back.
AD1CH15CONbits.TRG2SRC = 2;
// Select the AN5 analog positive input/pin.
AD1CH15CONbits.PINSEL = 5;
// Select signal sampling time (6.5 TADs = 81nS).
AD1CH15CONbits.SAMC = 3;
// Set ADC to RUN mode.
AD1CONbits.MODE = 2;
// Enable ADC.
AD1CONbits.ON = 1;
// Wait when ADC will be ready/calibrated.
while(AD1CONbits.ADRDY == 0);
// Trigger channel #15 in software and wait for the 123 samples
// accumulated result.
while(1){
// Trigger channel # 15.
AD1SWTRGbits.CH15TRG = 1;
// Wait for a conversion ready flag.
while(AD1STATbits.CH15RDY == 0);
// Read oversampling result. It will clear the conversion ready flag.
result = AD1CH15DATA;
}
return 1;
}