13.9.1.4 CPU Address Error Trap
This trap will be taken when any of the following circumstances occur:
- If a W-reg (W0 through W14) is used by an AGU as
a source or destination and a misaligned data word access (long word access at an
odd address or word access at an odd byte address) is attempted.Note: For misaligned writes, the read or write is not inhibited. Address alignment is forced such that read or write is always aligned.
- If a W-reg (W0 through W15) is used
by an AGU, and the address or offset pointed to by the W-reg is
beyond 24 bits in size. In other words, an address error trap will
be generated if the MSB of the address pointed to by the W-reg used
by the AGU is not set to 8'h00, or if the MSB of the address offset
pointed to by the W-reg, which is used for EA calculation, is not
8'h00 or 8'hFF.
or
as an offset where permitted and contains a value where the Most Significant 8 bits are neither 8’h00 or 8’hFF (the offset can be a signed negative value).Note: The CPU will detect X address access to SFRs and treat these as a special case. However, Y space reads of SFR or PS addresses must be detected by the BMX and result in an address error trap. - If the MSB of a computed PFC address
(
BRAW,RCALLW,CALLW,GOTOW) is not 8’h00.