14.2 Architectural Overview
A general-purpose I/O port that shares a pin with a peripheral is generally subservient to the peripheral. Once enabled, the peripheral selects whether the peripheral or the associated port has ownership of the I/O pin.
An MUX and its associated logic control interaction between peripherals and port logic. When a peripheral is enabled but the peripheral is not actively driving a pin, the port is still allowed to drive the pin. This is useful for “loop through,” in which a port’s digital output drives the input of a peripheral that shares the same pin.
When a peripheral is enabled and the peripheral is actively driving an associated pin, the IO MUX disables the use of the pin as a general-purpose output. The I/O pin value may be read by the port, but the LATx[n] output value for the port is ignored.
A block diagram of a typical I/O port structure is shown in Figure 14-1.