2.82.9 PORT_PinOutputEnable Function

C

void PORT_PinOutputEnable(PORT_PIN pin)

Summary

Enables selected IO pin as output.

Description

This function enables selected IO pin as output. Calling this function will override the MCC input output pin configuration.

Precondition

The PORT_Initialize() function should have been called.

Parameters

ParamDescription
pinOne of the IO pins from the enum PORT_PIN.

Returns

None.

Example

PORT_PinOutputEnable(PORT_PIN_PB03);

Remarks

None.