2.22.5 DAC_Channel1ResultGet Function
C
uint16_t DAC_Channel1ResultGet (void);
Summary
Returns the Channel 1 Filter output
Description
This function returns the value of the Channel 1 Filter output
Precondition
DAC_Initialize() function must have been called first.
Parameters
None.
Returns
result - Channel 1 Filter output
Example
uint16_t result = 0;
DAC_Initialize ();
result = DAC_Channel1ResultGet ();
Remarks
None.