2.13.4 CLC_CALLBACK Typedef

C

typedef void (*CLC_CALLBACK)( uintptr_t context)

Summary

Defines the data type and function signature for the CLC peripheral callback function.

Description

This data type defines the function signature for the CLC peripheral callback function. The CLC peripheral will call back the client's function with this signature when a CLC interrupt occurs.

Precondition

CLC_CallbackRegister must have been called to set the function to be called.

Parameters

ParamDescription
contextAllows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients)

Returns

None.