2.108.5 SEFCx_SectorErase Function
C
bool SEFCx_SectorErase( uint32_t address) // x - Instance of the SEFC peripheral
Summary
Erases a Sector in the FLASH.
Description
This function is used to erase a sector (collection of pages).
Precondition
Validate if SEFCx controller is ready to accept new request by calling SEFCx_IsBusy()
Parameters
| Param | Description |
|---|---|
| address | FLASH address to be Erased |
Returns
Always returns true.
Example
SEFC0_SectorErase(0x500000);
while(SEFC0_IsBusy());
Remarks
Application needs to poll for busy bit or wait for callback to be called before sending next request.