2.54.10 HSMCI_ResponseRead Function
C
void HSMCI_ResponseRead ( HSMCI_READ_RESPONSE_REG respReg, uint32_t* response )
Summary
Reads the specified response register
Description
Response of a command can be read using this API.
Precondition
A command having a response must have been submitted using the HSMCI_CommandSend() function.
Parameters
| Param | Description |
|---|---|
| respReg | Enumeration of type HSMCI_READ_RESPONSE_REG identifying the response register to read |
| response | Pointer to the buffer to read the response into |
Returns
None.
Example
uint32_t cmd_response;
HSMCI_ResponseRead(HSMCI_READ_RESP_REG_0, &cmd_response);
Remarks
None.