2.54.4 HSMCI_BlockCountSet Function
C
void HSMCI_BlockCountSet ( uint16_t numBlocks )
Summary
Sets the number of blocks to transfer
Description
Sets the number of blocks to transfer for a multi-block transfer. For example, the block count must be set to the appropriate value before issuing the multi-block read (CMD 18) or write (CMD 25) commands. For single blcok read (CMD 17) or write (CMD24) commands, the block count must be set to 1.
Precondition
HSMCI_Initialize() must have been called first.
Parameters
| Param | Description |
|---|---|
| numBlocks | Number of blocks to transfer |
Returns
None.
Example
HSMCI_BlockCountSet(1);
Remarks
None.