2.54.9 HSMCI_DataErrorGet Function
C
uint16_t HSMCI_DataErrorGet(void)
Summary
Returns the errors associated with a data transfer.
Description
Returns the errors associated with a data transfer. For a data transfer, the returned value is a bit wise OR of the errors defined in the HSMCI_ERROR_FLAGS enum.
The error flags are cleared after a call to this API.
Precondition
A command containing a data stage must have been initiated using the HSMCI_CommandSend() function.
Parameters
None.
Returns
Bit wise OR of the data error flags defined under the enum HSMCI_ERROR_FLAGS - HSMCI_DATA_TIMEOUT_ERROR, HSMCI_DATA_CRC_ERROR, HSMCI_DATA_UNDERRUN_ERROR, HSMCI_DATA_OVERRUN_ERROR.
Example
uint16_t data_error = HSMCI_DataErrorGet();
if (data_error & (HSMCI_DATA_TIMEOUT_ERROR | HSMCI_DATA_CRC_ERROR |
HSMCI_DATA_UNDERRUN_ERROR | HSMCI_DATA_OVERRUN_ERROR))
{
// Handle data error
}
Remarks
None.