2.54.8 HSMCI_CommandErrorGet Function
C
uint16_t HSMCI_CommandErrorGet(void)
Summary
Returns the errors associated with a command transfer.
Description
Returns the errors associated with a command transfer. For a command transfer, the returned value is a bit wise ORing of the following errors, defined in the HSMCI_ERROR_FLAGS enum.
The error flags are cleared after a call to this API.
Precondition
A command must have been initiated using the HSMCI_CommandSend() function.
Parameters
None.
Returns
Bit wise OR of the command error flags defined under the enum HSMCI_ERROR_FLAGS - HSMCI_CMD_TIMEOUT_ERROR, HSMCI_CMD_CRC_ERROR, HSMCI_CMD_END_BIT_ERROR, HSMCI_CMD_INDEX_ERROR.
Example
uint16_t cmd_error = HSMCI_CommandErrorGet();
if (cmd_error & (HSMCI_CMD_TIMEOUT_ERROR | HSMCI_CMD_CRC_ERROR |
HSMCI_CMD_END_BIT_ERROR | HSMCI_CMD_INDEX_ERROR))
{
// Handle command error
}
Remarks
None.