5.7.1.26 Text Option
The -mtext="scn-name[attributes]" option
places text (program code) in a section named
scn-name, rather than the default
.text section. Additionally, comma-separated attributes can be
specified along with the section name. No white space should appear around the
= character in this option.
For example, the following command line option redirects the
.text
section into a section called MySectionName and specifies its link
address.xc32-gcc bootloader.c -mprocessor=32MX795F512L -mtext="MySectionName,address(0x9D00a000)"This command is useful when used to map your code in a custom linker script as part of a bootloader project.