1.14 Pin Configuration

The I/O pins on the device can perform alternate functions besides the general-purpose I/O function. In this section, we will configure the functionality of the I/O pins needed for this demonstration.

  1. From the “Plugins” drop-down list, select “Pin Configuration”.
  2. Configure the pins for “SERCOM1” as shown below.
  3. Configure the pins for the “GMAC”.