1.18 Application Setup

  1. Establish a physical wiring with another 10BASE-T1S node as shown in the hardware setup picture below.
    Important: Both ends of the UTP cable must be connected to the PN port of the LAN867x and properly terminated with the jumper.
  2. Make sure that PLCA settings are correct.
  3. Make sure that Node Id, IP Addresses and MAC Addresses of the two nodes are different.

    There will be a virtual COM port enumerated when a Micro-USB cable from the computer is connected to the DEBUG USB port on the SAM E54 Curiosity Ultra Development Board [4].