2.3.8 Instantiating MiV ESS Core

To instantiate the MiV ESS core, perform the following steps:
  1. From the Catalog, drag the MiV_ESS IP core to SmartDesign.
  2. In the Create Component dialog box, enter MIV_ESS_C1 as the component name, and then click OK.
  3. In the MiV ESS Configurator screen, perform the following configurations:
    1. Navigate to General tab, and make sure that the configurations are same as shown in the following figure.
      1. Deselect Bootstrap.
      2. Select the following peripherals: GPIO, SPI, and UART, and deselect all others.
      Figure 2-16. General Configurator
    2. Navigate to APB tab, and enable APB Mirrored I/F as shown in the following figure.
      Figure 2-17. APB Configurator
    3. Navigate to GPIO tab, and make sure that the configurations are same as shown in the following figure.
      Figure 2-18. GPIO Configurator
    4. Navigate to SPI tab, and check the option of Keep SSEL active. Make sure that the configurations are same as shown in the following figure.
      Figure 2-19. SPI Configurator
    5. Navigate to UART tab, and make sure that the configurations are same as shown in the following figure.
      Figure 2-20. UART Configurator
  4. To generate the component, click OK.
The following figure shows the top SmartDesign after all the components are instantiated.
Figure 2-21. Top SmartDesign with All Components Instantiated