3.2.15.1 DIAG_MCLK_ClockCalibration
Returns the status of the MCLK_CLOCK_CALIBRATION diagnostic.
This function will perform frequency test on MCLK peripheral. This function will measure the frequency of the MCLK with reference clock.
DIAG_TEST_STATUS
DIAG_MCLK_ClockCalibration
(
uint32_t expected_mclk_freq
);
Diagnostic verifies the following faults do not exist
- MCLK is not generated properly
Operating Mode
- Interface can be used at POST
Precondition
- none
Parameters
- expected_mclk_freq - expected frequency of MCLK under test.
Returns
- DIAG_TEST_PASSED if no faults were found, otherwise, DIAG_TEST_FAILED.