3.2.9.4 DIAG_DSU_SFRReset
Returns the status of the SFR_RESET diagnostic
This function verifies correct reset values of each DSU peripheral register, by comparing the value of each register after reset, with the expected value stored in a table.
DIAG_TEST_STATUS
DIAG_DSU_SFRReset
(
uint32_t* reg_results,
uint32_t results_size,
bool dump_regs
);
Diagnostic verifies the following faults do not exist
- Control Register Failure
Operating Mode
- Interface can be used only at POST
Precondition
- None
Parameters
- reg_results - optional array of results
- results_size - size of results array
- dump_regs
Returns
- DIAG_TEST_PASSED if no faults were found, otherwise, DIAG_TEST_FAILED.