3.2.13.1 DIAG_GCLK_ClockCalibration
Returns the status of the GCLK_CLOCK_CALIBRATION diagnostic
This function will perform frequency test on GCLK peripheral. This function will measure the frequency of the GCLK with reference clock.
DIAG_TEST_STATUS
DIAG_GCLK_ClockCalibration
(
DIAG_GCLK_PERIPHS gclk_periph,
uint32_t expected_freq
);
Diagnostic verifies the following faults do not exist
- GCLK is not generated properly
Operating Mode
- Interface can be used at POST and ‘On Demand’
Precondition
- none
Parameters
- DIAG_GCLK_PERIPHS gclk_periph - glck peripheral
- uint32_t expected_freq - expected frequency
Returns
- DIAG_TEST_PASSED if no faults were found, otherwise, DIAG_TEST_FAILED.