13.32.10.1 Print Statement
Use the puts command to write a string to an output channel. Predefined output channels are “stdout” and “stderr.” If you do not specify a channel, then puts display text to the stdout channel.
Note: The STDIN Tcl command is not supported by Microchip tools.
Example:
set a [ myprog arg1 arg2 ]
puts "the answer from myprog was $a (this text is on stdout)"
puts stdout “this text also is on stdout”