13.32.10.2 Return Values
The return code of a Tcl command is a string. You can use a return value as an argument to another function by enclosing the command with square brackets [ ].
Example:
set a [ prog arg1 arg2 ] exec $a
The Tcl command “exec” will run an external program. The return value of “exec” is the output (on stdout) from the program.
Example:
set tmp [ exec myprog ] puts stdout $tmp