22.13.6 Add all Inputs to One Output Path Set
To show all inputs to one output you must configure and add the set to the Paths tab.
To create a set showing all inputs to one output:
- In the Paths tab, from the Edit menu, click Add Set of Paths. The Add Path Set dialog box appears.
- Select the Inputs and Outputs radio buttons.
- Click the directional arrow to point it left.
- Choose the desired output endpoint in the To list box.
- Select all inputs (all starting points), by Clicking on the Select All button under the From list box.
- Click OK. The set showing all inputs to one output is added to the Paths tab.