22.13.7 Edit or Remove a Path Set
To edit a path set:
- Select the set in the Paths tab.
- In the Edit menu, choose Edit Set of Paths, or right-click and choose Edit Set. This displays the Edit Set dialog box.
- Edit the Path Set and click OK.
To remove a path set:
- Select the set in the Paths tab.
- In the Edit menu, choose Remove Set of Paths, or right-click and choose Remove Set from the shortcut menu. The set is removed.