13.5.7 Source Files for Simulation

The Source Files for Simulation dialog box enables you to set the simulation file order in the Project Manager.

Figure 13-12. Organize Source Files for Simulation Dialog Box

De-select the Use default list from Project Manager checkbox to Add/Remove source files for simulation.

To specify the simulation file order:
  1. From the Project menu, choose File Organization > Source Files for Simulation. The Organize Source Files for Simulation dialog box appears.
  2. De-select the Use default list from Project Manager checkbox to Add/Remove source files for simulation. Click the Default button to reset the options to the original settings.
  3. Click OK.