13.5.6 Source Files for Synthesis

The Source Files for Synthesis dialog box enables you to set the synthesis file order in the Project Manager.

Figure 13-11. Organize Source Files for Synthesis Dialog Box

De-select the Use default list from Project Manager checkbox to Add/Remove source files for synthesis.

To specify the synthesis file order:
  1. From the Project menu, choose File Organization > Source Files for Synthesis. The Organize Source Files for Synthesis dialog box appears.
  2. De-select the Use default list from Project Manager checkbox to Add/Remove source files for synthesis. Click the Default button to reset the options to the original settings.
  3. Click OK.