This tutorial provides step-by-step instructions on how to program multiple Actel devices with
serialization. Before you begin this tutorial, you should already be familiar with the basic
features of the FlashPro® software.
Note: This tutorial does not provide software installation instructions. Please have FlashPro already installed before you begin.
In this tutorial you will program two devices in a chain (one device is A3P250 and the other is
A3PE600). The STAPL file for the first A3P250 device contains 10 serialization data. See
figure below.Figure 9-67. APA Device Tutorial Example
To create a new project:
Click the New Project
button in FlashPro.
From the New Project
dialog box, type "Tutorial" in the Project Name field.
Check the Chain box.Figure 9-68. New Project Dialog Box
If necessary, change the default location
of your project in the Project Location field.
Click OK. The
FlashPro main window appears and updates the Programmer List info with your programmer
information.
From the Programmers
menu, choose Scan Chain (or select the programmer in the Programmer
List window, right-click, then choose Scan Chain).Figure 9-69. Scan Chain Selection
Scan Chain shows how the devices are ordered in the chain in the log window. In
this case, A3P250 is the first device will be programmed in the chain since it is
connected directly to TDO.
Figure 9-70. Scan Chain Order in the Log Window
Click the Configure
Chain button . The Chain Configuration window appears.Figure 9-71. Chain Configuration Window
In the Chain
Configuration window, click the Add Device button to
add devices to the chain. The Add Actel Device dialog box
appears.
Choose A3P250 device
from the Device drop-down menu.Figure 9-72. Add Actel Device Dialog Box
In the STAPL file
field, use the Browse button to locate the A3P250.stp file.
In the Name field,
leave A3P250 as default.
Click OK. The A3P250
device is added into the Chain Configuration window.
Repeat steps 8 to 11 for A3PE600 and A3P250
respectively. After you are finished adding all devices in the chain, the Chain
Configuration window updates.Figure 9-73. Chain Configuration Window for all Devices
From the Chain
Configuration window, check the Enable Serial box. This
enables the Serial Data option in the Chain
Configuration window.
Click Select in the
Serial Data column, the Serial Settings
dialog box displays as shown in the figure below.Figure 9-74. Serial Settings Dialog Box
From the Serial
Settings dialog box, click the All button to select all
the serial data.
Click OK.
Once all the devices have been added to the
chain in the correct order and serialization has been selected, click the
Run button to program the chain.
When programming is complete, the
Programmer List window appears and indicates that the devices are
ready for programming.Figure 9-75. Programmer List Window Done
Congratulations! You have just completed the FlashPro Multiple Device Serialization Chain Programming tutorial.