9.5.5 Setting Disabled Actel Devices to HIGH-Z
This tutorial explains how to set disabled Actel IGLOO®, ProASIC3, SmartFusion®, Fusion and ProASICPLUS devices in a chain to HIGH-Z during chain programming.
Note: This tutorial requires a design with valid *.pdb/*.stp files for a chain of devices. If
you launch FlashPro® from a Libero® IDE project, a
FlashPro project is created automatically and the PDB/STP file loaded. Otherwise, you can
start a new FlashPro project and load a PDB/STP file; refer to the Chain Programming Tutorial for more information.
- Once all your devices have been added to the
chain, from the Chain Configuration window, choose which devices you
would like disabled during programming by de-selecting the appropriate checkbox from the
Enable Device column.
Now that you have disabled devices a checkbox appears in the HIGH-Z column of the Chain Configuration window. If the HIGH-Z column is not shown in the Chain Configuration Grid, right-click any column header and choose HIGH-Z.
- Select the HIGH-Z checkbox to ensure your
disabled devices enter HIGH-Z mode and remains in that mode until chain programming is
complete.HIGHZ is not supported if enabled Actel devices are executing one of the following ACTIONS:
- PROGRAM_NVM_ACTIVE_ARRAY
- VERIFY_NVM_ACTIVE_ARRAY
- READ_IDCODE