This tutorial demonstrates step-by-step instructions on how to parallel program two chains using
two programmers, each with two Actel Devices (A3P250 and A3PE600). See the figure below for an illustration.Figure 9-76. APA Device Tutorial Example
You should already be familiar with the basic features of the FlashPro®
software before you begin this tutorial.
Note: This tutorial does not provide software installation instructions. Please have FlashPro
already installed before you begin.
Click the New Project
button in FlashPro.
From the New Project
dialog box, type “Tutorial” in the Project Name field.
Check the Chain box.Figure 9-77. New Project Dialog Box
If necessary, change the default location
of your project in the Project Location field.
Click OK. The
FlashPro main window appears and displays your updated programmer information.Figure 9-78. FlashPro User Interface
From the Programmers
menu, choose Scan Chain (or select the programmer in the
Programmer List window, right-click, then choose Scan
Chain). The Select Programmer(s) dialog box displays.Figure 9-79. Select Programmer Window
The Programmer List window shows the Scan Chain Test was
passed and how the devices are ordered in the chain.
Figure 9-80. Scan Chain Order in the Log Window
Click the Configure
Chain button . The Chain Configuration window appears.Figure 9-81. Chain Configuration Window
In the Chain
Configuration window, click the Add Device button to
add devices to the chain. The Add Actel Device dialog box
appears.
Choose A3PE600
device from the Device drop-down menu.Figure 9-82. Add Actel Device Dialog Box
In the STAPL file
field, use the Browse button to locate the A3PE600.stp file.
In the Name field,
leave A3PE600 as default.
The A3PE600 device is added into the
Chain Configuration window.Figure 9-83. Device One Chain Configuration Window
Repeat steps 8 to 11 for A3P250. After you
are finished adding all devices in the chain, the Chain Configuration
window updates.Figure 9-84. Chain Configuration Window for all Devices
Once all the devices have been added to the
chain in the correct order and serialization has been selected, click the Run button
to program the chain.
When programming is complete, the
Programmer List window appears.Figure 9-85. Programmer List Window Done
Congratulations! You have just completed the FlashPro Multiple Device Serialization Chain Programming tutorial.