This tutorial provides step-by-step instructions on how to program multiple Actel devices in a
chain. You should already be familiar with the basic features of the FlashPro® software.
Note: This tutorial does not provide software installation instructions. Please have FlashPro already installed before you begin.
In the figure below, there are three devices in a chain (two A3P250 and one A3PE600). In this
section, we will program these three devices in the chain.Figure 9-58. APA Device Tutorial Example
To create a new project:
Click the New Project
button in FlashPro.
From the New Project
dialog box, type “Tutorial” in the Project Name field.
Check the Chain box.Figure 9-59. New Project Dialog Box
If necessary, change the default location
of your project in the Project Location field.
Click OK. The
FlashPro main window appears.
Note: The Programmer List window updates with your programmers
information.
From the Programmers
menu, choose Scan Chain (or select the programmer in the
Programmer List window, right-click, then choose Scan
Chain).Figure 9-60. Select Programmer Window
Scan Chain shows how the devices are ordered in the chain in
the log window. In this case, A3P250 is the first device that will be programmed in the
chain since it is connected directly to TDO.
Figure 9-61. Scan Chain Order in the Log Window
Click the Configure
Chain button. The Chain Configuration window displays.Figure 9-62. Chain Configuration Window
In the Chain
Configuration window, click the Add Device button to
add devices to the chain. The Add Actel Device dialog box appears.Figure 9-63. Add Actel Device Dialog Box
Choose the "A3P250" device from the
Device drop-down.
In the STAPL file
field, use the Browse button to locate the A3P250.stp file.
In the Name field,
leave A3P250 as default. The A3P250 device is added into the Chain
Configuration window.Figure 9-64. Device One Chain Configuration Window
Repeat the same process for A3PE600 and the
other A3P250 respectively.
After you have finished adding all of the
devices in the chain, the Chain Configuration window updates.Figure 9-65. Chain Configuration Window: All Devices in the Chain
Once all the devices have been added to the
chain in the correct order, click the Run button to program the
chain.
When Programming is complete, the
Programmer List window displays.
Figure 9-66. Programmer List Window Done
Congratulations! You have just completed the FlashPro Multiple Actel Device Chain Programming tutorial.