1.4.3 CFI Data

CFI Data is used to store the query data for CoreCFI. The data is stored in a reserved page location. This client does not take up any of the 2048 pages in the Flash Memory.

Use the dialog box to specify the location of the memory file for CFI query data (as displayed in the figure below). This memory file is provided to you when you obtain the CoreCFI IP. The memory file format is Binary. You are not expected to modify this file.

Figure 1-41. CFI Data Dialog Box
???

Output is top_level.vhd and top_level.efc if you use only the CFI Data client. The EFC file is used to program the Flash Memory System Builder.