1.4.5 RAM Initialization Client

You must create a RAM with Initialization core before it can be imported here.

When you generate a RAM with Initialization for Fusion, the data for the RAM can be loaded into the Flash Memory System Builder such that at power-up the data is loaded into the RAM from the Flash memory.

The difference between this and the regular Initialization Client is that the cascading of multiple RAM blocks is handled automatically. The RAM Initialization client takes as many initialization clients as there are RAM blocks in the cascaded RAM.

JTAG Protection protects your JTAG chain from reading and/or writing if you select the checkboxes.

You can also specify a start address and lock the start address if you wish to always use this address for initializing this client.

Figure 1-43. RAM Initialization Client Dialog Box
???