1.1.4.61 DRV_METROLOGY_SYN_DESCRIPTOR Struct

C

typedef struct {
    DRV_METROLOGY_SYN_CONTROL control;
    uint32_t *pData;
    struct DRV_METROLOGY_SYN_DESCRIPTOR *next;
    struct DRV_METROLOGY_SYN_DESCRIPTOR *prev;
} DRV_METROLOGY_SYN_DESCRIPTOR;

Summary

Data descriptor used to configure the synthesizer function.

Description

Field description:

  • control: Synthesizer control values. See DRV_METROLOGY_SYNTHESIZER_CONTROL.
  • *pData: Pointer to the data buffer with the waveform samples
  • *next: Pointer to the next descriptor address. If NULL, the descriptor is the last one to be performed.
  • *prev: Pointer to the previous descriptor address. If NULL, the descriptor is the first one to be performed.