37.7.45 USB LPM Attribute Register for LPM Transaction and Sleep Cycle

This register is used to define the attributes of an LPM transaction and sleep cycle. In both the Host mode and the Device mode, the meaning of this register is the same however the source of the data is different for Host and Device as follows:

In Device mode:

In Device mode, the values in this register will contain the equivalent attributes that were received in the last LPM transaction that was accepted. This register is updated with the LPM packet contents if the response to the LPM transaction was an ACK. This register can be update via software. In all other cases, this register will hold its current value.

In Host mode:

In Host mode software will set-up the values in this register to define the next LPM transaction that will be transmitted. These values will be inserted in the payload of the next LPM Transaction.

Table 37-47. Register Bit Attribute Legend
SymbolDescriptionSymbolDescriptionSymbolDescription
RReadable bitHCCleared by Hardware(Grey cell)Unimplemented
WWritable bitHSSet by HardwareXBit is unknown at Reset
KWrite to clearSSoftware settable bit——
Name: LPMATTR
Offset: 0x1360
Reset: 0x0000
Property: PAC Write-Protection

Bit 15141312111098 
 ENDPOINT[3:0]   RMTWAK 
Access R/WR/WR/WR/WR/W 
Reset 00000 
Bit 76543210 
 HIRD[3:0]LNKSTATE[3:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 

Bits 15:12 – ENDPOINT[3:0] LPM Token Packet Endpoint bits

This is the endpoint in the token packet of the LPM transaction.

Bit 8 – RMTWAK Remote Wake-up Enable bit

This bit is applied on a temporary basis only and is only applied to the current suspend state. After the suspend cycle, the remote wakeup capability that was negotiated upon enumeration applies.

ValueDescription
0Remote wake-up is disabled
1Remote wake-up is enabled

Bits 7:4 – HIRD[3:0] Host Initiated Resume Duration bits

The minimum time the host will drive resume on the bus. The value in this register corresponds to an actual resume time of:

Resume Time = 50 µs + HIRD * 75 µs. The resulting range is 50 µs to 1200 µs.

Bits 3:0 – LNKSTATE[3:0] Link State bits

This value is provided by the host to the peripheral to indicate what state the peripheral must transition to after the receipt and acceptance of an LPM transaction. The only valid value for this register is '1' for Sleep State (L1). All other values are reserved.