21.9.1 smartpower_add_new_custom_mode
(Ask a Question)Description
This Tcl command creates a new custom mode.
smartpower_add_new_custom_mode -name {mode name} \
-base_mode {base mode} \
[-description {mode description}]
Arguments
Parameter | Type | Description |
---|---|---|
name | string | Specifies the name of the new custom mode. This parameter is mandatory. |
base_mode | string | Specifies the name of the base mode used to create the new custom mode. It must be one of the following: Active, Standby or Flash*Freeze (RTG4, SmartFusion 2, and IGLOO 2). This parameter is mandatory. |
description | string | Specifies the description of the new custom mode. This parameter is optional. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'name' is missing. |
None | Parameter 'name' has illegal value. |
None | base_mode: Invalid argument value: 'mode_name' (expecting Active, Static, new_mode_name1, new_mode_name2 or new_mode_name4). |
None | Parameter 'base_mode' has illegal value. |
None | Required parameter 'base_mode' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_add_new_custom_mode -name "name" [-description "description"] -base_mode "Active | Static | new_mode_name1 | new_mode_name2 | new_mode_name4"'. |
Supported Families
Supported Families | Supported Versions |
---|---|
PolarFire® | v12.4+ |
SmartFusion® 2 | v12.4+ |
RTG4™ | v12.4+ |
IGLOO® 2 | v12.4+ |
PolarFire SoC | v12.6+ |
Example
This example creates a new custom mode "NewCustomMode" based on the Active mode:
smartpower_add_new_custom_mode -name {NewCustomMode} \
-base_mode {Active} \
-description {frequency 10 MHz}