Description
This tcl command adds a pin into a clock or set domain.
smartpower_add_pin_in_domain -pin_name {pin name} \
-pin_type {value} \
-domain_name {domain name} \
-domain_type {value}
Arguments
Parameter |
Type |
Description |
pin_name |
string |
Specifies the name of the pin to add to the domain. |
pin_type |
string |
Specifies the type of the pin to add. The acceptable values for this argument are the following:
- clock - The pin to add is a clock pin.
- data - The pin to add is a data pin.
|
domain_name |
string |
Specifies the name of the domain in which to add the specified pin. |
domain_type |
string |
Specifies the type of domain in which to add the specified pin. The acceptable values for this argument are the following:
- clock - The domain is a clock domain.
- set - The domain is a set domain.
|
Return Type |
Description |
None |
None |
Error Codes
Error Code |
Description |
None |
Required parameter 'pin_name' is missing. |
None |
Required parameter 'pin_type' is missing. |
None |
Required parameter 'domain_type' is missing. |
None |
Required parameter 'domain_name' is missing. |
None |
domain_type: Invalid argument value: 'value' (expecting clock or set). |
None |
Parameter 'pin_name' has illegal value. |
None |
Failed to add pin "pin_name" to "domain". |
None |
pin_type: Invalid argument value: 'value' (expecting clock or data). |
None |
Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_add_pin_in_domain [-pin_name "name of pin"]+ -domain_type "clock | set" -domain_name "name of domain" -pin_type "clock | data"'. |
Supported Families
Supported Families |
Supported Versions |
PolarFire® |
v12.4+ |
SmartFusion® 2 |
v12.4+ |
RTG4™ |
v12.4+ |
IGLOO® 2 |
v12.4+ |
PolarFire SoC |
v12.6+ |
Example
The following example adds a "XCMP3/U0/U1:Y" clock pin to an existing Clock "clk" domain:
smartpower_add_pin_in_domain -pin_name {XCMP3/U0/U1:Y} \
-pin_type {clock} \
-domain_name {clk} \
-domain_type {clock}
The following example adds a "XCMP3/U0/U1:Y" data pin to an existing Set "myset" domain:
smartpower_add_pin_in_domain -pin_name {XCMP3/U0/U1:Y} \
-pin_type {data} \
-domain_name {myset} \
-domain_type {set}