3.6.8.2.4 Step 4 - Open Serial UART Terminals
(Ask a Question)During the setup process you will need a couple of serial UART terminals to communicate with the PolarFireSoC: one for the HSS and another for the embedded Linux command line.
USB - UART Terminal
connection is made as described in3.6.8.2.1 Step 1 - Setup Required Board Connections.- Windows Users
- On Windows, To open the
HSS Serial Terminal
:- Open Interface 0 as shown below. Take note of the serial line number in parenthesis. In this case, Interface 0 is COM3. The digit could be different on your machine.If you encounter an issue configuring the serial connection to the board try the following:
- If you can’t find the serial port with the correct name, you may have to install CP210x Windows Drivers from SiLabs.
- You should be able to see the UART interfaces in . If you can’t, try selecting ,
- If you still can’t see the serial ports, then your USB socket could be broken, which is usually indicated if Windows makes no sound when disconnecting/reconnecting the USB cable.
. Select . Under Ports (COM & LPT), and look for “Silicon Labs Quad CP2108 USB to UART Bridge: - With the Icicle Kit on and connected, open a new PuTTY terminal. Change the settings on the left navigation panel, under
- Serial line to connect to: <Serial line number>
- Baud Rate: 115200
- Data Bits: 8
- Stop Bits: 1
- Parity: None
- Flow Control: None
to: - Go back to Session on the left navigation panel, Change Connection Type to Serial as shown below, then click Open:
- Open Interface 0 as shown below. Take note of the serial line number in parenthesis. In this case, Interface 0 is COM3. The digit could be different on your machine.
- Linux Users
- On Linux, to open the
HSS Serial Terminal
:- The UART channel that we will connect to is channel 0. To do this in GTKTerm, the command is:
sudo gtkterm -p /dev/ttyUSB0 -s 115200
Note that if you have other ttyUSB devices connected to your host PC, the number after
/dev/ttyUSb
may need to change. To out find which devices are associated with the Icicle Kit’s UART channels, you can runls /dev/ttyUSB*
with and without the USB cable connected to the board. Any new devices (there should be four) that appear when plugging in the board are the UART channels. For this step, we want to use the/dev/ttyUSB
device with the lowest number.
- The UART channel that we will connect to is channel 0. To do this in GTKTerm, the command is:
Embedded Linux Serial Terminal
To open the Embedded Linux Serial Terminal
follow the same instructions as the previous 3.6.8.2.4 Step 4 - Open Serial UART Terminals section. Except this time use interface 1 (/dev/ttyUSB1
on a Linux host PC, and Interface 1
on a Windows host PC).
In the example below, Interface 1 is on the COM4 serial line.