Description
This Tcl command renames a pin group on an instance in a SmartDesign component.
sd_rename_pin_group -sd_name {smartdesign component name} \
-instance_name {instance name} \
-current_group_name {current pin group name} \
-new_group_name {new pin group name}
Arguments
Parameter | Type | Description |
---|
sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. |
instance_name | string | Specifies the name of the instance on which the pin group is present. It is mandatory. |
current_group_name | string | Specifies the name of the pin group to be renamed. It is mandatory. |
new_group_name | string | Specifies the new name of the pin group. It is mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'sd_name' is missing. |
None | Required parameter 'instance_name' is missing. |
None | Required parameter 'current_group_name' is missing. |
None | Required parameter 'new_group_name' is missing. |
None | Parameter 'param' is not defined. Valid command formatting is 'sd_rename_pin_group -sd_name "sd_name" -current_group_name "current_group_name" -new_group_name "new_group_name" -instance_name "instance_name"'. |
SDCTRL05 | Pin 'MyGroup' does not exist. |
None | Parameter 'current_group_name' has illegal value. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This command renames "Group" to "MyNewGroup" on the "COREAXINTERCONNECT_C0_0" instance in the "TOP" design:
sd_rename_pin_group -sd_name {TOP} \
-instance_name {COREAXINTERCONNECT_C0_0} \
-current_group_name {Group} \
-new_group_name {MyNewGroup}
See Also
- sd_create_pin_group
- sd_add_pins_to_group