Description
This Tcl command renames an instance name in a SmartDesign component. This command can be used to
rename any type of instances (instances of other SmartDesigns components, core
components, HDL modules, HDL+ cores and Microchip macros) in a SmartDesign.
Note: This command is not required to build a SmartDesign component. It command maps to an interactive user action in the SmartDesign Canvas and will not be present in the exported SmartDesign component Tcl description.
sd_rename_instance -sd_name {smartdesign component name} \
-current_instance_name {instance name} \
-new_instance_name {new instance name}
Arguments
Parameter | Type | Description |
---|
sd_name | string | Specifies the name of the SmartDesign component in which the instance name has to be renamed. It is mandatory. |
current_instance_name | string | Specifies the name of the instance to be renamed. It is mandatory. |
new_instance_name | string | Specifies the new instance name. It is mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Parameter 'new_instance_name' has illegal value. |
None | Parameter 'current_instance_name' has illegal value. |
None | Required parameter 'sd_name' is missing. |
None | 'Instance name' has been duplicated, please specify a different name. |
None | Instance 'instance_name' does not exist. |
None | The first character of '*' must be a letter. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_rename_instance -sd_name "sd_name" -current_instance_name "current_instance_name" -new_instance_name "new_instance_name"'. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command renames "DFF_0" instance name with a new "DFF_1" name in the 'top' SmartDesign
sd_rename_instance -sd_name {top} \
-current_instance_name {DFF_0} \
-new_instance_name {DFF_1}