Description
This Tcl command removes synthesis attribute from the specified net of the specified SmartDesign.
sd_remove_net_synth_attr \
-sd_name {SmartDesign component name} \
-net_name {net name} \
[-attr_name {synthesis attribute name}]
Arguments
Parameter | Type | Description |
---|
sd_name | string | This argument is used to specify the name of the SmartDesign component from which the net synthesis attribute is removed. This is a mandatory argument. |
net_name | string | Name of the net in SmartDesign from which synthesis attribute is removed. This is a mandatory argument. |
attr_name | string | Synthesis attribute to be deleted. If the argument is not specified all the attributes are deleted. |
Synthesis Attributes
The following is the list of attributes and directives available in the Synopsys® FPGA synthesis tool that are supported by SmartDesign.
Name |
Object |
Attribute/Directive |
syn_insert_buffer |
port, instance |
Attribute |
syn_keep |
net |
Directive |
syn_maxfan |
port, net, instance, register |
Attribute |
syn_no_compile_point |
module/architecture |
Attribute |
syn_noclockbuf |
port, net, module/architecture |
Attribute |
syn_noprune |
instance, module/architecture |
Directive |
syn_preserve |
register, port, module/architecture |
Directive |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Failed to remove synthesis attribute 'syn_keep' from the net 'net_name'. This attribute does not exist. |
None | Net 'net_name' does not exist. |
None | Parameter 'net_name' has illegal value. |
None | Required parameter 'net_name' is missing. |
None | Parameter 'attr_name' has illegal value. |
None | Parameter 'sd_name' has illegal value. |
None | Required parameter 'sd_name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_remove_net_synth_attr -sd_name "sd_name" [-attr_name "attr_name"] -net_name "net_name"'. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example removes "syn_keep" attribute of "CLK" net in the "top" design.
sd_remove_net_synth_attr -sd_name {top} \
-attr_name {syn_keep} \
-net_name {CLK}