Description
This tcl command resets the canvas layout of the given SmartDesign.
sd_reset_layout \
-sd_name {SmartDesign_component_name}
Arguments
Parameter | Type | Description |
---|
sd_name | string | Specifies the name of the SmartDesign on which the layout will be auto arranged. It is
mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code |
Description |
None |
Required parameter 'sd_name' is missing. |
None |
The component 'SmartDesign_component_name' does not
exist. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example resets the canvas layout of the given SmartDesign.
sd_reset_layout -sd_name {sd}