21.4.22 sd_delete_instances

Description

This tcl command deletes one or more instances from a SmartDesign component.

Note: This command is not required to build a SmartDesign component. This command maps to an interactive user action in the SmartDesign Canvas and will not be present in the exported SmartDesign component Tcl description.
sd_delete_instances -sd_name {smartdesign component name} \
                    -instance_names {instance names}

Arguments

ParameterTypeDescription

sd_name

string

Specifies the name of the SmartDesign component. It is mandatory.

instance_names

string

Specifies the instance names to be deleted. It is mandatory.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
None

Parameter 'instance_names' has illegal value.

None

Required parameter 'instance_names' is missing.

None

Parameter 'sd_name' has illegal value.

None

Required parameter 'sd_name' is missing.

None

Parameter 'param_name' is not defined. Valid command formatting is 'sd_delete_instances -sd_name "sd_name" -instance_names "[instance_names]+"'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4
SmartFusion® 2
IGLOO® 2

Example

This example deletes "RAM64X12_0" instance.

sd_delete_instances -sd_name {top} \
                    -instance_names {RAM64X12_0}

See Also

  • sd_disconnect_instance
  • sd_duplicate_instance