Description
This tcl command adds one or more pins to a pin group on an instance in a SmartDesign component.
sd_add_pins_to_group -sd_name {smartdesign component name} \
-instance_name {instance name} \
-group_name {group name} \
-pin_names {pin names}
Arguments
Parameter | Type | Description |
---|
sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. |
instance_name | string | Specifies the name of the instance on which the pin group is present. It is mandatory. |
group_name | string | Specifies the name of the group to add the pins to. It is mandatory. |
pin_names | string | Specifies the list of instance pins to be added to the pin group. It is mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_add_pins_to_group -sd_name "sd_name" -instance_name "instance_name" [-group_name "group_name"] [-pin_names "[pin_names]+"]'. |
None | Required parameter 'sd_name' is missing. |
None | Required parameter 'instance_name' is missing. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example adds "ARESETN" and "CLK" pins to the Group of "COREAX_C0_0" instance in the "top" design:
sd_add_pins_to_group -sd_name {top} \
-instance_name {COREAX_C0_0} \
-group_name {Group} \
-pin_names {ARESETN ACLK}
See Also
- sd_create_pin_group
- sd_remove_pins_from_group