4.6.34 Wind/U Error: Failed to connect to the registry on server

Symptom: The following error message appears:
Wind/U Error: Failed to connect to the registry on server [server_name]

Cause: There might be a Linux security setting that is preventing Libero from connecting to the Wind/U Registry. Typically, this connection is made using a TCP port.

Resolution: Perform the following procedure:
  1. Modify the Linux security settings. For example, on RHEL5, navigate to the desktop menu System > Administration > Login screen > Security tab, and uncheck Security Setting Deny TCP connections to Xserver.

  2. Restart your computer to apply the changes.